Smart Smoke Detector

The Netatmo Smart Smoke Detector is a photoelectric (optical) technology based device that increases the level of security in your home. When the Smoke Detector detects a fire, it immediately sends an alert directly to your smartphone. This way you can react even when you are away from home.

Real-time alerts on your smartphone

Are you away from home? If so, you won’t even hear the loudest 85 dB fire alarm. Unlike traditional devices, the Netatmo Smart Smoke Detector eliminates this problem by sending real-time fire alerts straight to the smartphones belonging to you and your family.

10-year battery life*.

Many people forget to replace dead batteries in smoke detectors because they have to do it too often. But with this arrangement, can you be sure that everything will work as it should when a fire breaks out?
The Netatmo Smart Smoke Detector has a special built-in battery that lasts for 10 years*, which means you don’t have to worry about powering the detector for a whole decade. This corresponds to the lifetime of the sensor itself, so during this time any fire will be noticed in time. After 10 years, it is recommended to replace all smoke detectors with new ones.

No low battery warnings for a full decade*.

Are you woken up by persistent low battery alerts on your smoke detector? With the Netatmo Smart Smoke Detector, you can rest easy and not worry about powering it for a whole decade*.

Low battery warning

The Smart Smoke Sensor sends you alerts on your smartphone when the battery is nearing the end of its 10-year lifespan*, which means the unit needs to be replaced.

Sound check reminders

The app allows you to set monthly, semi-annual or annual reminders to test your Smart Smoke Detector. As recommended, such a check should be performed at least once a year.

Hassle-free installation

No more troublesome alarm wiring. Just mount the wireless Smart Smoke Detector on the ceiling and download the app, and in no time your home is protected from fire. It’s that simple.

Where to install the Smart Smoke Detector?

For safety and protection from fire, install a Smart Smoke Detector in all bedrooms, children’s rooms and hallway. For added safety, additional Smart Smoke Detectors may be installed in the living room, attic and basement. In some countries local regulations may also apply. Please refer to the regulations for smoke detectors.

Automatic diagnostics

Do you sometimes wonder if your home smoke detector is working properly? The Smart Smoke Detector constantly monitors the battery status, checks the performance of the smoke detection mechanism and checks Wi-Fi connectivity. If there are any technical problems, you will receive a notification on your smartphone.

Silencing the alarm with a smartphone

Alarm went off because of burnt toast? You don’t have to climb on a chair to turn off the ceiling-mounted device – just mute the Smart Smoke Detector alarm with your smartphone.

Standalone product

The Smart Smoke Detector is a completely stand-alone product. It doesn’t need an expensive smart home management panel to work.

Smart Smoke Detector for complete protection

Optical (photoelectric) smoke detector

85-decibel audible alarm when smoke is detected

Wi-Fi connectivity for remote alarm triggering

Built-in batteries for up to 10 years*

Built-in status LED

Bluetooth Low Energy (BLE) technology for remote Hush functionality and HomeKit interoperability

*Life span under standard use. It is subject to change depending on how the Smart Smoke Detector is used. Additional information can be found at: https://netatmo.com/usage/nsd